2019-12-07 5:44 AM
Hy all,
I have a little problem. I am using a B-G431b-ESC1 developement kit. I generated a code with the help of Motor control Workbench and MX. I followed the steps from:
At section 6.1, step 7 : " the motor starts to rotate respectively" but mine just BEEP-ing.
If I push the reset button on the daughter board, the motor starts to rotate and after 2-3sec stops and naturally, resets the MCU.
My question is, why my motor does not rotating using this generated code? I attached my code, thank you for helping
2020-09-10 7:41 AM
Dear N
It is a rather old post.
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-09-22 1:41 AM
Dear N
OK. I consider this post closed.
Do not hesitate to answer if it is not.
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.