2020-11-03 9:13 AM
I am using NUCLEO-F303RE, X-NUCLEO-IHM08M1, MotorControl Workbench 5.4.4 and STM32CubeMX 5.5.0. I have managed to generate a project as position control and it seems to work fine however I am wondering if I can improve further the performance of the motor by fine tuning the PID controller (for now I just tried some random values). Each parameter of the PID has a divider associated with it and I would like to know how this affects the performance. Once the code is generated the dividers are the followings:
#define SP_KPDIV 16384
#define SP_KIDIV 16384
#define SP_KDDIV 16
#define SP_KPDIV_LOG LOG2(16384)
#define SP_KIDIV_LOG LOG2(16384)
#define SP_KDDIV_LOG LOG2(16)
it is obvious that the LOG has the same value, but what if I change this how will it affect the performance. what values are best to be used?
Thanks in advance for your help.
2020-12-31 8:09 AM
Dear @msingh
Sorry for the late answer.
Do you have still this problem to solve?
And just in case, if not, do not hesitate to share the final solution you found. Thanks by advance.
Best regards
Laurent Ca...
2021-01-18 1:58 AM
Dear @Laurent Ca... ,
Yes I still haven't understood properly how the divider works, is there any documentation you can suggest?
Kind Regards
Manpreet Singh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.