STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! ST motor control evaluation kit (FOC)

This is the first time in this forum and want to start working on the ST micro controller. My main aim is a. Buy high end ST evaluation kit and understand the FOC algorithm for PMSM motors. The kit should contain the motor along with evaluation kit.b...

VD.3 by Associate II
  • 3435 Views
  • 5 replies
  • 0 kudos

Six-Step BLDC Control Complimentary Switching Issue

Hello, Currently, I'm working with BLDC motor controller development. I used complementary switching logic to control my MOSFET. Here, the motor is not starting at less duty cycle, the motor is starting only at 70percent duty cycle. and more noise al...

How to add a custom chip in the X-Cube-MCSDK?

I have a controller based on STM32F303VDT7 chip and want to use MCSDK with it, but there is no this particular chip in the SDK. I can`t found any directory with .svd files or any other way to add my chip. Is there any way to do it?

AKons.1 by Associate
  • 1072 Views
  • 1 replies
  • 0 kudos

B-G431B-ESC1 does not respond to PPM input

Hello, I generate a 4.4V 1400us on (2000-1400)us off signal and verify its existence with scope. This signal does not induce movement in the motor I have attached to the ESC evaluation board.The board beeps using the motor when powered on. When I con...

sspry by Associate II
  • 6773 Views
  • 11 replies
  • 0 kudos

Hi, I am using B-G431B-ESC1 Discoery kit to run the BLDC Maxon Motor. I am encountering problem with this discovery kit that it is not able to run the motor. Motor and hall sensors are all good as I have tested with other BLDC controller.

I have configured the Motor workbench and generated the C code firmware for B-G431B-ESC1 and I can read input voltage and Hall sensors when I rotate the motor manually with hand. I am having problem with PWM signals from micrcontroller that it makes ...

MAsif.1 by Associate II
  • 6251 Views
  • 6 replies
  • 0 kudos

[STEVAL-001V1, SPEED FEEDBACK FAULT] How to tune MC for high-speed motor, getting speed feedback fault on high RPM

I'm evaluating the STEVAL-ESC001V1 and I finally got the code to compile correctly and I'm able to run a hobby RC BLDC at 3-shunt sensorless mode.However I'm facing an issue with high RPMs with motor stopping and ESC giving speed feedback fault. This...

jiso by Associate
  • 2343 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.