2020-02-12 6:21 AM
I'm evaluating the STEVAL-ESC001V1 and I finally got the code to compile correctly and I'm able to run a hobby RC BLDC at 3-shunt sensorless mode.
However I'm facing an issue with high RPMs with motor stopping and ESC giving speed feedback fault. This happens systematically when trying to push the motor above 15.5k RPM. Maximum RPM of the motor is 20k.
I have ran the motor profiler and verified the values by manually measuring those according to ST instructions. Motor parameters are correct, so what should be the next steps to try to overcome the issue? Should I start tuning the sensorless speed management settings to be able to run the motor on max RPM? Or do you have some tuning guideline document that I could follow?
2020-09-11 2:15 AM
Dear Jiso
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-09-23 4:04 PM
Dear @jiso
I guess you don't have to solve this problem anymore, therefore I consider this post closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...
2021-04-10 9:06 AM
Hello,
I have the same problem with a B-G431B-ESC.
Someone have some advices?
Thanks
Orso
2021-04-13 4:16 PM
Hello,
I'm observing that I have this problem only when I put a propeller on my motor.
Using the MC_GetOccurredFaultsMotor1() function I see that the fault are double.
It seems that OVERCURRENT FAULT and SPEED FEEDBACK Fault comes at same time.
Since that happens at higher speeds with propeller I'm begin to think that the speed feedback
fault can be a sequence of a real overcurrent fault. By the way the maximum current of
my motor is 25A while the board support 45A if I'm not wrong, and the profiler as no
problem to profile my motor with propeller at full speed. So strange...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.