STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! EVSPIN32G4 Works once

Hello, I’m working with an EVSPIN32G4 demo board and trying to get it running with a Bodine BLDC motor in a sensorless (hall-less) configuration. I’ve got firmware that appears to work initially, but after pressing RESET or cycling the 48 VDC power, ...

RinSxi by Associate
  • 446 Views
  • 1 replies
  • 0 kudos

P-NUCLEO-IHM001 Motor Kit Usage

I am currently seeking to implement motor rotation control to any desired angle using the P-NUCLEO-IHM001 motor kit. Is this feasible? If so, how should I proceed? Are there any relevant tutorials or documentation available? Thank you. *This post has...

Issue with Workbench 6.4 and Motor Profiler

I've gotten myself into an odd bug or something. I had been using the Motor Profiler successfully from the Workbench for a month or so and I had to stop for a while and work on other items. I may have played around the graphing/plotting stuff in Moto...

PMSM Current waves

Hi. I used steval-ipm15b and nucleo-g431 to run a pmsm motor. when I see the current waves in the motor pilot or osciloscope, they are not sinus-shaped waves. can anyone help me what is the problem and what should I do?

Analog servomotors with F334R8

Hi everybody!I started programming ARM microcontrollers after watching Mr. Patrick Hood-Daniels' tutorials on YouTube. I am using a Nucleo F334R8 development board to control a Puppet animatronic I am making for my niece. You can see it here:https://...

SkelePaw by Associate
  • 463 Views
  • 0 replies
  • 0 kudos

New to STM32F446 and IHM08M1

Hai All,   Got a STM32F446 & IHM08M1.   Planning to do the six step commutation using High/Low Method (without PWM), Hall Effect Sensor & Timer.   What are the precautions to be considered?    Any links..

Stepper Control with l6474

Hi, @Peter BENSCH . I am working on a project. In which i need to control Stepper motor using X-Nucleo-IHM01A1 Sheild. Currently i'm using STM32G431RB Nucleo-64 board for this and in future will use STM32F103. I've download X Cube SPN1 for basic work...

SannanAli by Associate II
  • 2016 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.