STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Problems with SDK3.2 and MCWB 2.0

Posted on September 14, 2012 at 02:21I have an IPMM with absolute position resolver mounted on it. Unfortunately i can not use it even with decoder - absolute position to 12-16 bit paralel interface. Thats why i try to run in sensorless modes with 2...

FOC SDK V3.2 confidential distribution

Posted on October 02, 2012 at 11:51I have changed FOC SDK V3.0 to work with a linear motor with analog hall sensor and these changes work so far with the STM32F103RC microcontroller. But actually I have planned to use STM32F205RB microcontroller for...

fortunat by Associate II
  • 1568 Views
  • 3 replies
  • 0 kudos

3Phase Induction Motor with FOC SDK3.2

Posted on November 04, 2012 at 11:19Hello... I do want to have motion contol with 3Phase induction motor with FOC algorithm. The FOC library(FOC SDK v3.2--UM1052) and software(ST Motor Control WorkBench) offered ST is for PMSM. I dont want to use Pe...

saraaj100 by Associate II
  • 4710 Views
  • 9 replies
  • 0 kudos

Has STM32 MC FOC SDK V3.3 released?

Posted on December 13, 2012 at 00:37Hi, I noticed that  STM32 MC FOC SDK V3.3 was mentioned in ST Motor Control Workbench V2.1 as one of the target libraries. I also found a http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/REL...

tamil by Associate II
  • 1663 Views
  • 3 replies
  • 0 kudos

IHM023V2: FOC duration fault

Posted on February 07, 2013 at 14:11Hardware: STEVAL-IHM023V2 + STM32100B-EVAL + custom motor Configuration: High-voltage 3-phase PMSM, IAR 6.50.2.4585, STM32 PMSM FOC Firmware Library v3.2 - WEB distribution I'm trying to get started with the examp...

STM3210B-MCKIT Hall Sensor or Encoder

Posted on March 12, 2013 at 11:10hi, I got the STM3210B-MCKIT and use the 3.2 FOC Lib + Workbench 2.0. I tried to get the Encoder control to work: - I jused the SDK32x-STM3210B-EVAL-MB459-Shinano.stmc - under Drive Management I changed the sensor s...

Error for foc sdk v3.2

Posted on March 28, 2013 at 16:47 Hello, I compile the library foc sdk v3.2 with Atollic for stm32f100b and with gnu I have always the same error : C:\VSS\MC\3PH\012\SOFTWARE\FIRMWARE\MC SDK v3.3\MC library\src\MotorPowerMeasu...

Error for foc sdk v3.2

Posted on March 28, 2013 at 16:48 Error for foc sdk v3.2 Hello, I compile the library foc sdk v3.2 with Atollic for stm32f100b and with gnu I have always the same error : C:\VSS\MC\3PH\012\SOFTWARE\FIRMWARE\MC SDK v3.3\MC...

ST Motor Control Workbench V2.1

Posted on April 03, 2013 at 02:56 Where can I find workbench version 2.1? In a previous thread entitled '' Has STM32 MC FOC SDK V3.3 released?'', theST Motor Control Workbench V2.1 is mentioned.On this page, I found Version 2.0 of the Motor...

lumley by Associate II
  • 1376 Views
  • 2 replies
  • 0 kudos

STM32F100C8T6BTR

Posted on May 11, 2013 at 12:11Hello, I'm using the ''STM32F100C8T6BTR'' to control motor with sensorless mode with enable low side signals. I have always the same error '' Foc duration'' (Foc Sdk v3.2 and 3.3) The frequency is '' 12500 Hz'' and I'm...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.