2013-03-28 8:48 AM
Error for foc sdk v3.2
Hello,
I compile the library foc sdk v3.2 with Atollic for stm32f100b and with gnu I have always the same error :C:\VSS\MC\3PH\012\SOFTWARE\FIRMWARE\MC SDK v3.3\MC library\src\MotorPowerMeasurementClass.c:(.text+0x34): undefined reference to `__aeabi_memclr'
Do you have an idea for this error ?
Thank you,
2013-03-29 1:11 AM
Ciao Julien,
I thnik that you are triyng to mix to much! I read v3.2 one line and v3.3 in the next. Moreover the WEB distribution has been released with the compiled part compatible just with IAR so if you want to do the porting on Atollic is necessary that you start from the sources. If you request is justified with a businnes you can try to get the source code contacting your nearest ST office. Ciao Gigi2021-06-21 9:27 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.