2017-11-09 3:23 PM
When running the potetiometer example on the ST motor control workbench, there is an initial ramp up before it settles to the value based on the ADC reading of the potentiometer. Is there a way to remove this so that it always follows the potentiometer?
2021-06-27 6:31 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.