STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Integer conversion resulted in trucation - ID_DEMAG

Posted on March 31, 2014 at 21:32I am receiving this compiler error in SystemNDrivePrarms.h on lines 8182, 8216, and 8250 when compiling MCTasks.c.  (MC version: 3.4.1, IDE: IAR EW for ARM 7.10)  ID_DEMAG,        /*!< Demagnetization current in s16A...

luke23 by Associate III
  • 2535 Views
  • 5 replies
  • 0 kudos

Can I use the MC monitor with our custom board?

We have developed our own MC board, based on STM32F303 Nucleo-64 with some different pinout. We do not have integrated ST-LINK like the Nucleo board of course, just a JTAG connector. Can we use our custom board in combination with the MC monitor? Whe...

CPrin by Associate III
  • 2516 Views
  • 5 replies
  • 0 kudos

How to get one PWM output inverted?

I have the Shinano motor running correctly with the NUCLEO-F303RE board and the X-NUCLEO-IHM08M1. I'm trying now to get it working with our custom board. Unfortunately my hardware colleagues have used the NCP5304 bridge driver instead of the L6398 dr...

CPrin by Associate III
  • 2327 Views
  • 3 replies
  • 0 kudos

STEVAL_IHM042V1 | DUAL | FOC 4.3 | AC6

Posted on October 28, 2017 at 14:31Hi,which user AC6 project can be used in combination with STEVAL_IHM042V1?I would like to use the STEVAL_IHM042V1 to run two motors with hall sensorsIs it: \Web\Project\AC6\STM32F30x_UserProject -> config STM32303C...

paul2 by Senior
  • 3425 Views
  • 7 replies
  • 0 kudos

ST MCWB BusVoltageSensor error

Posted on August 09, 2017 at 13:44Hi. I am using MCWB with FOC 4.3. with STSPIN32F0 eval board. I am trying to switch on the bus voltage sensing. When I set it in the WB, compile and upload, it always randomly pops under or overvoltage error. I can ...

ICS Current sensing problem

Posted on February 29, 2016 at 20:28We use the motor control library STM32 PMSM FOC V4.2 .For current control using 2 ICS, but of all the formula to calculate the current , torque used  value of Rshunt(Ohm) and AmplificationNetworkGain. Current[A] =...

vad_21 by Associate
  • 1238 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.