2019-10-19 4:50 PM
HI
ANY ONE KNOW HOW CAN START AC INDUCTION MOTOR WITH SDK5 LIBRARY OR ST HAVE LIBRARY FOR AC INDUCTION MOTOR
Solved! Go to Solution.
2021-06-28 5:45 AM
Dear @omid hamdi
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2019-12-19 7:36 AM
Hello Omid,
I am also looking for answer to this question. Do let me know if you got some pointers.
Thanks
Narendra
2019-12-24 4:10 PM
HI
OLD have ac with encoder v5 cannot support ac sensorless st plan in future add ac sensorless on library still cant support
if u need check ti website have more sample for ac induction bout if you need used st controller you must write program with your self
best regards
2019-12-24 8:27 PM
2020-01-17 5:36 AM
Dear Omid and NKale,
We know the AC Induction motor control is missing in our library... Sorry about this! Anyway, the team keeps working to add day after days new features and SW. Please keep posted
Claire
2021-06-15 1:07 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2021-06-28 5:45 AM
Dear @omid hamdi
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.