STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

STM32F746G-Disco

HiCan you make an application for 2 axis motor control and reading from 2 position encoders on the STM32F746G-Disco?Andrzej

+/- 1 RPM Resolution using B-G431B-ESC1 Discovery Kit

I have this kit, am using the MCSDK under STM32CubeIDE, and everything seems to be functioning fairly well. I'm still getting the occasional fail to start issue, but what I'm really trying to do is to be able to specify motor speed +/- 1 RPM, and be ...

GHave.1 by Associate II
  • 1818 Views
  • 2 replies
  • 0 kudos

What to change in FOC code for lower inertia?

I have a BLDC motor running reliably with FOC code on a STM32G431 MCU. For unrelated mechanical reasons we need to drop our inertia by about 4x from where it is running today. For the speed loop I fully understand lowering inertia raises the loop ga...

BTrem.1 by Senior II
  • 1731 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.