2021-10-29 12:22 AM
I want to change few parameters detected by motor profiler in my code(After code generation) But i don't want to change it manually..I am trying to changes in pmsm_motor_parameter.h . Can you tell me which files are used to write parameters from motor profiler?I want to test wide range of value change of parameters and it effect on motor behaviour
Solved! Go to Solution.
2021-10-29 1:01 AM
Hello @Tejashree
We do not recommend you to change the generated files manually.
Our recommandation is to change the motor parameters with the workbench and generate your project from the workbench.
If your own code is inside USER SECTION (as the one I proposed you yesterday) it will be kept during project generation.
Regards
Cedric
2021-10-29 1:01 AM
Hello @Tejashree
We do not recommend you to change the generated files manually.
Our recommandation is to change the motor parameters with the workbench and generate your project from the workbench.
If your own code is inside USER SECTION (as the one I proposed you yesterday) it will be kept during project generation.
Regards
Cedric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.