STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Problem building the example with EVSPIN32F0251S1 board

Using the EVSPIN32F0251S1 board, I tried to use the example in the STSW-SPIN32F0251 library but I can't get 6 Steps commutation with Hall Effect sensors to build. Here are the steps that I have tried : Download libraryUnzip the fileGo Projects/EVALST...

MDoyo.2 by Associate
  • 950 Views
  • 1 replies
  • 0 kudos

Problem with downloading X-CUBE-MCSDK-FUL

I have registered and was trying to download X-CUBE-MCSDK-FUL. When I clicked on any of the versions (5.5.3, 5.5.2, 5.4.7) a pop-up window appears for me to type in various info. I was able to enter all requested info, except "application", which a...

LChan.12 by Associate
  • 1044 Views
  • 1 replies
  • 1 kudos

ADC issue (possible bug) using IHM042v1

I have problems with Bus Voltage Sensing on IHM042v1. I'm trying to get it to work with 2 motors, both using encoder. I moved ENC_Z/H3_B signal to pin PA6 and Bus Voltage Sensing to pin PB2(ADC2_IN2)/PB12(ADC4_IN3) (tried both) leaving ENC_A/H1_A on ...

Z0ld3n by Associate
  • 1140 Views
  • 1 replies
  • 0 kudos

How to adjust the parameters of the en.X-CUBE-SPN7_v1.1.0 template program is that the sensorless BLDC speed reaches 60000 rpm

I am currently using the x-Nucleo-IHM07M1 (or P-NUCLEO-IHM001)development board to drive a brushless DC motor. I downloaded the en.X-CUBE-SPN7_v1.1.0 template program. I found that the program can reach up to 36000 rpm and then it can’t be improved, ...

0693W00000Hnb7oQAB.png
杨REN.1 by Associate
  • 1970 Views
  • 3 replies
  • 1 kudos

STEVAL-IHM023V3 MotorControl Workbench 5.Y.2 ACIM

Hi..I am trying to drive an ACIM motor on a project with STEVAL-IHM023V3 using Nucleo STM32G431RB MCU, but in some cases when starting the motor, a phase explodes and Rshunt ,IGBT, driver ,(sometimes) Nucleo STM32G431RB are destroyed.I did some resea...

Omer Ab by Associate III
  • 1772 Views
  • 1 replies
  • 0 kudos

Few questions regarding ST Motor Control

Hi, I have few questions regarding ST motor control library and hardware/motor compatibility.I need to control two high speed / low inductance Maxon Motors (ECX SPEED 8 M Ø8 mm) using position control (encoder) . Is steval-ihm042v1 inverter board suf...

Z0ld3n by Associate
  • 1803 Views
  • 2 replies
  • 0 kudos

Interrupt value does not get reset

I am using timer 4 in STM32G431 to read hall sensor input and trigger interrupt when high ..Above is my setting.void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){ if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) { _hallA = HAL_TIM_ReadCapturedV...

0693W00000Hof0yQAB.png 0693W00000Hof1XQAR.png 0693W00000Hof27QAB.png
Tejashree by Associate III
  • 2174 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.