STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

TIMER doesnt work when i link the lcd

#define TRIAC_PULSE_WIDTH 500 // Duration of TRIAC trigger pulse in µs   lcd_init();   lcd_send_cmd (0x80|0x00); lcd_send_string("HELLO WORLD");   lcd_send_cmd (0x80|0x40); lcd_send_string("LCD 20x4 DEMO");   lcd_send_cmd (0x80|0x1C); l...

LFerr.7 by Associate II
  • 3928 Views
  • 8 replies
  • 0 kudos

Resolved! NUCLEO-F302R8 not found in MC workbench?

I have a NUCLEO-F302R8 that I am trying to configure via the Workbench, but there are only 5 control boards shown in the new project setup screen:NUCLEO-G071RBNUCLEO-G431RBNUCLEO-G474RESTM32G081B-EVALSTM32G474E-EVALThats not a lot of options, so what...

SSeve.2 by Associate
  • 1488 Views
  • 2 replies
  • 1 kudos

How can I generate an .stmcx file without the GUI?

I have several .stmcx files to generate projects for. I don't have the time to open, generate, and wait for each one to generate. Is there a way to automate this process, preferably through Windows command line or Linux Terminal, though writing a C...

DSchu.9 by Associate II
  • 1053 Views
  • 1 replies
  • 0 kudos

IPM driver

I am trying to find / create a program to run an IPM module that will run an a/c compressor(PMSM). Like a MC3PHAC 6 pwm generator.Never written a program before except change some values to make the led blink faster.Have a NUCLEO-F401REIPM module: PS...

suicune by Associate
  • 1680 Views
  • 2 replies
  • 0 kudos

Resolved! FOC software and motor drive hardware

I would like to control a low voltage three phase BLDC motor using field oriented control with an STM32 microcontroller and appropriate motor drive hardware.is there a solution available from ST to start to this development like a motor drive expansi...

IAher.1 by Associate
  • 1342 Views
  • 1 replies
  • 0 kudos

I have a couple questions: 1. Is there a document with a description of the motor control registers? 2. Is there a library that I can import into my project to support comms between an STM motor controller/inverter board and a master device?

I found the following document: STM32F PMSM single/dual FOC SDK v4.3.This has a section (14) which has some explanation to how serial comms with a motor control device can work. There is even a list provided of "relevant motor control registers", how...

mike_ee1 by Associate
  • 1306 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.