2022-07-13 1:32 PM
I have several .stmcx files to generate projects for. I don't have the time to open, generate, and wait for each one to generate. Is there a way to automate this process, preferably through Windows command line or Linux Terminal, though writing a C, C++, Python, Java, etc. is also workable.
All I need to do is generate. I do not need to change any parameters or configure anything, just click the generate button and wait the ~2 minutes for it to generate.
Thanks.
2022-07-15 7:58 AM
Hello @DSchu.9,
I recommend you following the steps described in the 3.3.2 section of the UM1718.
Thank you.
Chahinez.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.