2022-07-06 5:30 AM
I have a NUCLEO-F302R8 that I am trying to configure via the Workbench, but there are only 5 control boards shown in the new project setup screen:
Thats not a lot of options, so what am I missing to get support for all the other micros?
Solved! Go to Solution.
2022-07-06 8:36 AM
Hello @SSeve.2 ,
The MCSDK 6.0.0 is limited to a few boards. It is the reason why the MCSDK 5.Y is still available for download. We plan to release a 6.1.0 which will support all the 5.Y boards, and even more.
Regards
Cedric
2022-07-06 8:36 AM
Hello @SSeve.2 ,
The MCSDK 6.0.0 is limited to a few boards. It is the reason why the MCSDK 5.Y is still available for download. We plan to release a 6.1.0 which will support all the 5.Y boards, and even more.
Regards
Cedric
2022-07-15 10:57 AM
Any further news on when this might be? I too have the same issue - using MCSDK 5.Y is fine, but that means a whole new load of installs and additional (and possibly outdated) firmware and drivers etc.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.