STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Porting Project to Pin Compatible MCU in STM32CubeIDE

I am currently working on a motor controller project with the STM32G473RE.I am trying to get more prototype boards made but the STM32G473RE is not in stock anywhere with long lead timeI see that the STM32G474RC has plenty of stock in multiple locatio...

KYin.2 by Associate II
  • 7679 Views
  • 4 replies
  • 0 kudos

Resolved! How to run a motor using ST Motor Pilot 6.1.1

similar question as https://community.st.com/s/question/0D53W00001wHk5BSAS/motor-wont-start-with-motor-pilotI am trying to run a BLDC motor using Motor Pilot 6.1.1 with B-G431B-ESC1.Here's my process.profile motor using motor profilergenerate code us...

_legacyfs_online_stmicro_images_0693W00000bkQUlQAM.png
JKong.3 by Associate III
  • 3070 Views
  • 1 replies
  • 0 kudos

My question is, is it possible view the given PWM to the GATE pin of high side MOSFET via microcontroller pin or the PWM logic is controlled by the logic circuit i.e inside of the STSPIN.

We are trying to use STSPIN32G4 Evolution board for our ventilator air blower driver application.We are facing the problem that we are receiving Speed feedback error while we connect our motor with STSPIN board via ST's Motor Driver Workbench (Motor ...

rkuma.21 by Associate III
  • 4532 Views
  • 6 replies
  • 0 kudos

Resolved! Open Loop Mode in MCSDK

I have seen the following options in the software in MCSDK  MCI_CMD_SETOPENLOOPCURRENT, /*!< set open loop current .*/ MCI_CMD_SETOPENLOOPVOLTAGE, /*!< set open loop voltage .*/in mc_interface.h file, but i don't see any source code related to them d...

SRedd.5 by Senior III
  • 8355 Views
  • 13 replies
  • 0 kudos

Resolved! How do I operate motor profiler from Motor Pilot V1.1.5?

Whenever I detect boards, the software tells me it needs to update the firmware on the target. Then it pops up a dialog that says it is checking ST-Link connection. However, it says in this state forever without error or progress. How can I either in...

MAnde.11 by Associate III
  • 6405 Views
  • 10 replies
  • 1 kudos

Resolved! No USB enumeration of STEVAL-SPIN3201

I am attempting to use an STEVAL-SPIN3201 eval board for the first time but cannot get it to enumerated on USB. LD2 flashes slowly indicating the embedded ST-LINK is operating. I have tried installing the Windows driver using en.stsw-link009, but no ...

DHemb.1 by Associate II
  • 1495 Views
  • 1 replies
  • 0 kudos

Open loop Current Mode B-G431B-ESC1

Thank you for support till now, i want to do the open loop current mode using the B-G431B-ESC1 software. This is the code i have writtenif(g_motormodeselection_u8 == OPENLOOP_CURRENTMODE )    {    MC_SetCurrentReferenceMotor1(g_qdreference_s);    M...

SRedd.5 by Senior III
  • 1180 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.