STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

NUCLEO-G431RB + IHM08M + HALL, tried many different combination of KP and KI still no luck to make my motor spin

MCSDK 5.4.8 profiler work and MCWB work, code generated.Motor is able to spin under MCWB, but even HALL option is selected, MCWB is spin without HALL and therefore its generated code is not aiming for HALL startup right? I tried many different combin...

Implement Six Step -FOC Switch Over

Hello Community,I am sure about everyone being aware of the classic initial encoder alignment error in FOC. I am trying to bypass the entire alignment procedure by a method using calculated angle from Hall Sensors. I plan to run the motor initially i...

ASaha.3 by Associate
  • 1306 Views
  • 1 replies
  • 0 kudos

SPI encoder implementation.

HiI am looking for hints - how to implement the encoder from which I read the position via SPI?Should I set the encoder with index in Motor Control Workbench? If so, where to write the position read after SPI to "pretend" an ordinary encoder? I also ...

JStrz.1 by Associate
  • 2497 Views
  • 3 replies
  • 1 kudos

Connection error

Hi all.I use Nucleo-F746ZG, X-Nucleo-IHM07M1 and Maxon motor (https://www.maxongroup.com/maxon/view/product/motor/ecmotor/ecflat/ecflat45/668555). These boards were purchased separately.Motor Profiler and Motor Pilot give a connection error. CubeIDE ...

0693W00000UnZGqQAN.png 0693W00000UnZHeQAN.png
Borys by Associate
  • 1627 Views
  • 1 replies
  • 1 kudos

Resolved! Debuggers for Motor control

Hi,   I have been using STM-STUDIO-STM32 for moitoring the real time variable while motor running without disturbing the program.  MCU used - Stm32F103c8t6 Debugger used - st-link v2 Software used - Stm-stdio  - The stm-stdio is get stopped while deb...

Bud by Associate III
  • 2058 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.