STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Motor profiler MCSDK 6.2.0

I am moving to MCSDK 6.2.0 and want to test the motor profiler new feature. [VERSION]: MCSDK 6.2.0[TOOL]: Motor PROFILER v1.2.4EVALSTDRIVE101 + NUCLEO-F746ZG + Custom board for adapter[DETAILS]: Fail to do motor profiling[EXPECTED BEHAVIOR]:  Able to...

APerr.3 by Associate II
  • 2439 Views
  • 2 replies
  • 0 kudos

Implement brake mode and avoid overvoltage

Hi,[VERSION]: MCSDK 6.2.0[TOOL]: SDK Application Code: - single PMSM Motor- FOC- Sensorless Cordic - on STM32 G4- on the fly startup enabled- flux weakening enabled- speed controller[DETAILS]:We have a fan application with large mechanical energy and...

SF??r by Associate III
  • 3323 Views
  • 3 replies
  • 0 kudos

DRV8313 simplefoc

Hello all developers. I have a wish for you to start developing. simplefocmini (drv8313pwpr) with stm32cubeide I understand the basics of using a 3 phase timer. By creating a 120 degree difference, I can make the motor rotate but it is unstable.And I...

non by Associate III
  • 3742 Views
  • 3 replies
  • 0 kudos

Make work a board STEVAL-SPIN3204

Can anyone tell me how to do to make work a board STEVAL-SPIN3204?I've tried many version of Motor Control Workbench, build the exemple for SPIN3204, for STM32cubeIDE, and for Keil V5... But it never works!!!Is there anybody who success to make work ...

fDUMA.1 by Associate
  • 1105 Views
  • 1 replies
  • 0 kudos

Resolved! EVSPIN32F02Q1S1 SPI Interface

Hello,I have a EVSPIN32F02Q1S1 and I am attempting to communicate between the EVSPIN32F02Q1S1 and another device over SPI (Jetson Nano running Linux/Ubuntu). I was looking into using spidev to communicate but I cannot seem to find any details or info...

Failed to execute MI command

Hello, I have a problem with running code, generated by motor workbench:Guess it is not hardware problem, because i can run another project on it. Error in final launch sequence: Failed to execute MI command:load C:\\Users\\tomek\\OneDrive\\Dokumenty...

Tomuello by Associate II
  • 2871 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.