2024-02-14 10:34 PM - edited 2024-02-15 12:06 AM
Hello,
I have an EVSPIN32G4-Dual, I am Trying to Run 2 HooverBoard Motors (36V/15A/510RPM/HALL).
I generated the firmware using Mc Workbench 6.2.1 and desabled the overcurrent protection for stage 2.
Then tried to command the motors using motor pilot, turning each motor separately work fine,
But trying to turn one after the other, the 2 motors start shaking (didn't even start turning) ending up with one of them turning off or both, with an error of Over current in stage 1 and driver protection in stage 2.
Is there anyone used this board and managed to run 2 motors simultaneously.
Thank you in advance.
2024-02-19 6:50 AM
Hello,
Thank you for this problem report.
We are investigating the issue, and we will come back to you asap.
2024-03-01 1:21 AM
Hello,
Could you please check the following post and try the proposed modifications to check if it improves your use case behavior?
Evspin32G4 - dual - STMicroelectronics Community
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.