STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

MCSDK MCU

Hello everybody, i am new in ST. I am designing my own ESC.It is a control of a high power motor (950V, 400A Peak) to a BLDC / PMSM motor. I am designing my own power part and I need advice about the logic part, which NUCLEO is the best???Parameters:...

Vlad_ESC by Associate
  • 1909 Views
  • 2 replies
  • 0 kudos

STM32446RE with Stepper Motor Driver L6470 IC

HelloI understand the Nucleo 401 board was developed with the l6470 stepper motor driverI have been trying to interfacel6470 it with the nucleo 446re arm, with very little joy,... actually no joy due to the very poor C code support from ST and the L6...

JHERI by Senior
  • 2012 Views
  • 1 replies
  • 0 kudos

Unable to read data from L6470 Motor Driver

I m using STM32L552ZE as SPI Master and slave device is L6470 stepper driver. Write operation everything is fine. While i tried to read the data from STATUS Register (0x19) or GETSTATUS register(0xD0). I received only floating values not a constant o...

Resolved! is anything wrong in my invert.json?

I'm working on a custmoize inverter board .and I wan't to use Three-Shunt variants for current sensing, I implemented it in hwVariants, according to the documentation.See the following :{ "type": "inverter", "name": "testNow", "descVersion": 4,...

截屏2024-03-28 19.11.18.jpg 截屏2024-03-28 19.10.48.jpg

P-NUCLEO-IHM03 can't works

Hi st team,I have purchase the P-NUCLEO-IHM03  development kit, i am using the development as the follows:1, MotorControl workbench 6.2.12, STM32CubeMx 6.10.03, STM32CubeIDE1.14.1 I have try the follow steps:1,In MotorControl workbench 6.2.1 i follow...

swingboard_0-1711086435395.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.