STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

b-g431b-esc1 Overcurrent at the start

I have a custom motor controlled with the b-g431b-esc1 that I have been able to run in position control mode without overcurrent protection. As soon as I activate overcurrent protection the motor goes in the fault state when I click the "start" of th...

giova_ by Associate II
  • 1373 Views
  • 1 replies
  • 0 kudos

IHM14A1

Hello,I would try to use  the IHM14A1 shield  and  for now i only have a nucleo F2 series . it seemed in the document that this nucleo is not supported , can somebody tell me if it can't works  or maybe with some modifications on the example code. th...

Resolved! Motor Control Protocol Suite Library

Hi everybody,I was looking at the documentation for the MCSDK6 (great work btw), in particular to the Motor Control Protocol Suite section.Everything is well documented, however, I was wondering if is there any DLL available in order to facilitate th...

Resolved! dynamically changing Timer ARR and CCR1

Hi everyone,I am currently working on controlling a stepper motor using a PWM signal. I want to dynamically update the speed of the motor using different ARR and CCR1 values. Controlling the stepper works fine until an uncertain amount of time when t...

Smar by Associate II
  • 3313 Views
  • 2 replies
  • 1 kudos

ST Board with inline phase current (AN5423)

Hello. I am just starting in the world of motor control with ST parts and SW, so please be patient with me.I have checked different motor control boards for BLDC, and some related documentation, and I found special interesting the AN5423.https://www....

PCota by Associate
  • 1956 Views
  • 1 replies
  • 0 kudos

Resolved! EVLSPIN32G4-ACT Evaluation Board CAN-FD

Hello,   I bought two EVLSPIN32G4-ACT motor control evaluation boards and tried to setup CAN-FD communication between them.   Then I came to know it doesn't have a CAN transceiver IC(U3) populated on board. Image attached for your reference.   Can an...

YBhat.4 by Associate II
  • 1756 Views
  • 1 replies
  • 1 kudos

I recently started using ST Motor Control Workbench,Every time I try to generate FOC, I end up with this Error always "MotorControl Reference Pack not found."

I've tried reinstalling the software multiple times, also tried to generate FOC using its Previous version but same result. and also, I tried searching for Reference pack, but I couldn't find it. Is there anything I might be doing wrong......? I'm Us...

0693W00000bkRRnQAM_Screenshot 2023-05-19 161839.png
Vishnu by Associate II
  • 2376 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.