STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

What are the maximum motor electrical parameters?

What's the maximum/minimum electrical parameters for the motors that can be used with the MCSDK?Especially the important parameters like winding inductance and resistance values.We're trying to get a motor to run that has a Stator Resistance of 0.011...

DMeie.2 by Senior II
  • 807 Views
  • 0 replies
  • 0 kudos

CubeMX Project breakdown

Hello everyone, I ran into a problem when re-generating a project in a СubeMX.If I make some updates in the peripheral settings and generate a project in the mx cube, my build goes through without errors and warnings. But if I load this project into ...

Sergiu_Pascari_0-1715682803583.png Sergiu_Pascari_1-1715682865499.png

Motor control FOC sensor-less startup problem

Hi all!I'm currently developing my own motor control board and have encountered a problem with running the FOC algorithmI can’t understand how the motor should start correctly in sensorless mode. At the moment, when first starting, the program period...

bus current

I would like to implement a feature,During motor operation,Increasing loads,By controlling the rotational speed,so that when the bus current reaches a given value, it does not increase any further,What should I do?

iskan by Associate III
  • 910 Views
  • 0 replies
  • 0 kudos

Motor profiler and NUCLEO-G474RE (IHM16M1)

I plan to start using the MC SDK, and I was ready to get a Nucleo-G474RE with a IHM16M1.But when looking at the motor profiler utility, I noticed that the combination is not supported. There is support for the IHM16M1 and the STM32G474 processor in t...

ACarr.4 by Associate
  • 2001 Views
  • 2 replies
  • 0 kudos

Workbench connection failed

Hi all. Today our custom design board just arrive and we begin to test. Our custom board controllinng via STM32F103RBT6 product and programmed through the Stlink programmer using Stlink Utility software. We have a problem about connection using COM p...

qqwq.1 by Associate II
  • 2194 Views
  • 3 replies
  • 0 kudos

Resolved! About x-cube-mcsdk ver.6.2.1 and nucleo-h745zi

I set up x-cube-mcsdk least ver.6.2.1 workbench with a combination of nucleo-h745zi(motor control board) and x-nucleo-ihm08m1(motor inverter board).The pin configuration is the default setting.Where should I connect x-nucleo-ihm08 to nucleo-h745zi?

RIG by Associate III
  • 3146 Views
  • 4 replies
  • 2 kudos

about the charge boot capacitor time and duty

hi,    I set the charge boot capacitor time with 100ms and the duty with 50%. the picture is below, and I captured the waveform by the scope. low side (green,16V from drive circuit),high side (red, 3.3V from MCU). the low side boot time is 125us. why...

截屏2024-04-02 12.52.36.jpg 截屏2024-04-02 12.54.56.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.