2024-04-25 3:31 AM
Hello,
I would try to use the IHM14A1 shield and for now i only have a nucleo F2 series . it seemed in the document that this nucleo is not supported , can somebody tell me if it can't works or maybe with some modifications on the example code.
thanks
jerome
2024-05-06 1:41 AM
Hello @Jerome_DataP and welcome to the ST Community.
From the hardware point of view you can use a Nucleo F2 series board to drive the X-NUCLEO-IHM14A1 shield.
You can use generic GPIO to drive the motor driver expansion board.
There are no libraries ready for this pair of boards, in fact the X-CUBE-SPN14 software is compatible with a selection of Nucleo board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.