STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

MCSDK 6.3.0 is out!

Dear MCSDK users, MCSDK version 6.3 is now available: Download It here. Here are the main changes for this version: Motor Control Features: FOCAdded C0 single shunt topology support.6StepThis algorithm has been enhanced on MCSDK version 6.3 release ...

GMA by ST Employee
  • 4488 Views
  • 1 replies
  • 4 kudos

Understanding PLL State Observer

Hardware: EVSPIN32G4-DualMotors: 2x Moons BLDC R57BLB50L2, Hall-effect sensors not connected or desired.Application - 2x BLDC on shared timing pulley (no slip) system.  1:1 pulley ratio between motors.  Goal: equal load distribution between the two m...

ccut93 by Associate III
  • 3802 Views
  • 1 replies
  • 0 kudos

Resolved! How to test motor current ADC working properly?

We're currently having issues with our inverter.To further analyze the issue, I'd like to test the proper function of the motor phase current measurement.How should I go about doing that? Since the motor currents are measured in injected mode syncron...

DMeie.2 by Senior II
  • 1993 Views
  • 2 replies
  • 1 kudos

Resolved! Motor Pilot application is not starting

The Motor Pilot 6.0.0 application is not starting. I have testet it on Windows 10 on a real machine and on a Windows 10 virtual machine. When I start the application the course briefly shows that the machine is working but then nothing happens. No er...

MLang.7 by Associate III
  • 5963 Views
  • 9 replies
  • 0 kudos

Resolved! EVSPIN32G4-DUAL Second Motor will not spin

Hello,I am trying to evaluate the use of MCSDK in a dual-motor application.  Motor 1 works, but motor 2 does not.I have a fresh Workbench project, with both motors configured identically, with the exception of Over-Current Protection.  When I generat...

ccut93 by Associate III
  • 3004 Views
  • 2 replies
  • 0 kudos

Resolved! Asymmetric Serial Packet Exchange Protocol

We have been told Asymmetric Serial Packet Exchange Protocol documentation would be available with the release of MC Workbench V6. We're at V6.3 now. Can you direct me to where I might find said documentation?The old serial communication class availa...

JELLY.1 by Associate II
  • 1983 Views
  • 2 replies
  • 1 kudos

Trouble with MC SDK and NUCLEO-H745ZI-Q / X-NUCLEO-IHM07M1

Hi everyoneAre there any experiences with Motor Controll SDK 6.2.1 with NUCLEO-H745TI-Q and extension Board X-NUCLEO-IHM07M1?I try to get a basic FOC - Speed controller running on my NUCLEO-H745ZI-Q. But I struggle  completely.Something goes wrong. N...

adkr by Associate
  • 1175 Views
  • 1 replies
  • 0 kudos

Resolved! Evspin32G4 - dual

Hello All,I just Bought an Evespin32G4 dual Board.https://www.st.com/en/evaluation-tools/evspin32g4-dual.html I completed the configuration using the X-CUBE-MCSDK-6.Goal: I will command 2 motors 36V, 4A (Moteur Hoverboard)I generated the cube ide pro...

ItzSam by Associate II
  • 4991 Views
  • 8 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.