STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Where does G431 TIM1 ITR1 acturlly from?

Hello everyone! I use a BLDC with hall sensors drivered by ST's B-G431B-ESC1 inverter board, and demo code generated by MC Workbench. Use ST Motor pilot V1.2.5 - MC_FOC_SDK have a test, BLDC is runing and everything is ok. In the demo code, TIM4 use ...

xiepan_1-1715054384150.png xiepan_2-1715054420279.png
xiepan by Associate
  • 1525 Views
  • 1 replies
  • 0 kudos

Motor Control Help - EVLDRIVE101-HPD

Hi,I can't manage to get my motor to work with the EVLDRIVE101-HPD board. I have generated the FOC firmware and uploaded it to the board through STM32CubeIDE. See attached for main.cIs there something else I need to do? I have followed everything in ...

mitch1 by Associate II
  • 7976 Views
  • 10 replies
  • 0 kudos

Why the start of ovm mode is set to these value?

#define OVM_VREF_MODE1_START ((int32_t)29717) #define OVM_VREF_MODE2_START ((int32_t)31186)The ratio between these two value is not sqrt(3)/2. What is the voltage unit used in these calculation? Or when a have a Valpha equal to 32767, what is the tru...

Konecho by Associate II
  • 1367 Views
  • 2 replies
  • 0 kudos

B-G431B-ESC1 not connecting to Motor Pilot

I have crated a start project for the B-G431B-ESC1 using MC Workbench 6.3.0I used the following settings:Motor 'Bull Running BR2804-1700kV' and Inverter 'B-G431B-ESC1' the project User Interface show ON for 'Over USART A' at 115200 baud.I can build c...

murpia by Associate II
  • 2719 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.