STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Motor Workbench 6.2.1

Hi, I'm currently using Motor Workbench 6.2.1 and I'm trying to create a new project with a custom power board. To that end, I want to create the JSON descriptor file of the board.I have read the "Motor Control Boards description format" manual from ...

RTira.1 by Associate II
  • 2424 Views
  • 2 replies
  • 0 kudos

STM BLDC Motor Driver with BLE Control/ DFU

Hi,I am prototyping a custom PCB with integrated ESC for a BLDC Motor (Datasheet attached). For this purpose, I plan of using STSPIN32F0 due to versatile options following this article. The article's design is based on 45A max consumption and looking...

x4ce by Associate III
  • 1267 Views
  • 0 replies
  • 0 kudos

Motor hold with 6-step algorithm

I'm building a motor for position control with a command rate ~10 Hz.  I'm using MCSDK 6.2.1 with a 6-step algorithm and Hall sensors.  The motor has a gear drive ratio ~400:1.  The output shaft has a rotary encoder for position.  I use the standard ...

CraigH by Associate
  • 1469 Views
  • 1 replies
  • 0 kudos

MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL fails to compile

Hi,MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL fails to compile with the errors below: C:/Users/Ian/.st_workbench/projects/MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL/Src/mc_tasks.c: In function 'MC_RunMotorControlTasks':C:/Users/Ian/.st_workbench/projects/MCSDK-PKG00...

murpia by Associate II
  • 1188 Views
  • 1 replies
  • 0 kudos

Resolved! Questions on roadmap for ACIM supoport

Hello,I am considering transitioning to the ST MCU family for my inverter projects. The primary type of motor I use is ACIM. From what I have read, the latest version of the MCSDK/MotorControl Workbench only supports ACIM through two examples, and it...

Paiva404 by Associate
  • 2324 Views
  • 2 replies
  • 0 kudos

Tutorial -STEVAL-SPIN3202/STEVAL-SPIN3204

Hello Team,   we try to run the motor using motor control work bench, STM mx and STM cube IDE. motor run for 3 to 5 sec and stop.Is there any tutorial or any document or example we can follow step by step and understand each parameter related to STEV...

Sayali23 by Associate II
  • 1275 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.