2024-10-07 5:01 AM - last edited on 2024-10-07 5:57 AM by Andrew Neil
Hi. I'm using the STM32F407VE6 Microcontroller board. Is it possible to use a single timer to generate PWM from channel 3 and read the encoder values from channel1 & 2 of the same timer?
When I tried using 2 different timers, one for PWM and the other for the encoder it worked fine.
If it's impossible to use the same timer for both operations, why are channels 3 and 4 available for PWM generation?
2024-10-07 5:12 AM - edited 2024-10-07 5:13 AM
Timers have a single counter register. You cannot use a timer for an encoder and for PWM at the same time.
2024-10-07 6:29 AM
> If it's impossible to use the same timer for both operations, why are channels 3 and 4 available for PWM generation?
Even with the counter clocked from the encoder, you may find uses for the compare features, including the functionality which is called PWM. You may for example want generate a pulse when a rotary encoder rotates through some portion of its path.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.