2023-05-10 8:01 AM
I'm using ST Motor Pilot V1.1.5 with eval board B-G431B-ESC1.
Motor: IBL-100SW-1 http://www.itomotor.com/product/detail/67.html
Motor Profiler Configuration:
Pole Pairs: 3
Max Speed: 2000 RPM
Max peak current: 5 A
Magnetic: I-PMSM
ld/Lq: 1
After starting the profiler, the motor tries to start. But then, after a few seconds the profiler stops and shows the fault message "Over Voltage". This happens even if supply voltage is only 12 V. The oscilloscope shows that PWM peak voltage starts with 12 V and then rises up until more than 30 V between GND and motor phases.
2023-08-22 7:20 AM
Hello @Marc1 ,
I would be happy to help you if you still need. Have you tried with the latest version of MCSDK 6.1.2. If not, have you tried lowering the amperage on the profiler?
Regards
2023-08-28 12:56 AM
Hello @Zied b.,
I used the latest version of MCSDK at that time. It was MCSDK 6.1.1. I have tried lowering current and voltage.
2023-08-28 1:01 AM
Hello @Marc1
We made some changes on 6.1.2 can you try and tell me if it works better?
Regard
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.