2026-01-16 1:55 AM - last edited on 2026-01-16 2:00 AM by mƎALLEm
Hello everyone,
as part of a project, I would like to control a NEMA 17 or 23 stepper motor via UART. A TMC2209 driver is being used, and the software environment is STM32 CubeIDE. For reasons we cannot explain, we are unable to get the motor running.
I am open to any tips that could help us get the motor working. The code can also be provided if needed.
Thanks in advance for all feedback :)
2026-01-16 2:10 AM
Hello Lucas and welcome to the ST community,
Read also a related thread here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.