2021-06-15 10:21 PM
I download "STSW-SPIN3204" and compile with Keil .When open the project . Warming message shows"FrameworkCubeMX.gpdsc"is missing.
How to solve it?
2021-06-27 7:55 PM
Dear @kelvin.wang
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
2021-06-28 11:41 PM
Dear Sir,
HW is steval-spin3204 with 18V BLDC motor.
FW is download from ST website ""STSW-SPIN3204"".
IDE is uVision V5.34.0.0.
I just extract the FW and follow the Getting start document to open the multi-project. Then the "FrameworkCubeMX.gpdsc" error message shows and open a window to open the CubeMX.
I think that is some file missing in the Demo FW.
Also , I had installed the MCSDK 5.Y.1 and try the Demo code for SPIN3204 EVB. The process seems good (Generate code-->compiler--->upload to EVB). But I still can't spin my motor. The Motor Pilot tool shows "Over current". I had check all setting with circuit and setting for over current protection and even remove the OCP . But the result still the same OVER CURRENT protect.
MCSDK example name "6S_STEVAL3204_HS_VM"
Please help ,thank you!!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.