2021-06-23 4:28 PM
I have a motor with delta windings and in initial testing with MCSDK it doesn't seem to work. Looking at the current feedback on a scope and it looks awful compared to a similar wye winding motor on-hand with similar specs.
Before investing more time into the issue I want to verify that MCSDK should work fine with delta windings
Hardware:
STM32F446RE nucleo board
X-NUCLEO-IHM07M1
Both motors using 2048-count encoders for feedback
Thanks in advance!
Solved! Go to Solution.
2021-06-30 9:59 PM
Dear @TGers.1
Yes, STM32 MC-SDK works fine with delta windings.
In fact, STM32 MC-SDK is dependent neither on motor structure nor connection schemas.
Differences are only on main motor family types.
Best regards
2021-06-30 9:59 PM
Dear @TGers.1
Yes, STM32 MC-SDK works fine with delta windings.
In fact, STM32 MC-SDK is dependent neither on motor structure nor connection schemas.
Differences are only on main motor family types.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.