2019-05-22 9:59 AM
Hello,
I have a problem that I don't know to solve and any help will be appreciated very much.
I'm working with STM32L476RCT, and BOOT0 is configured to 0 to boot from flash. The NRST state is also correct.
My problem is when I program the mcu, the code seems to not start. The execution only starts if I do a hardware reset in NRST pin. It also doesn't work when I power up from power off. The code only works if I force a hardware reset (NRST = 0).
I'm sure that is a problem of the firmware because I have tested the MCU with other code and it works properly. I'm working with Eclipse Workbench.
Any tip or indication will be a big help to me.
Thank you very much,
Luis
2019-05-22 10:32 AM
If BOOT0 is pulled low, it probably is running your code.
Are there things on the board that may power up slower, or take time to start?
Consider a POR circuit if you have multiple power rails.
Make sure you've instrumented any Error_Handler() or HardFault_Handler() type routines where it could go into a while(1) and silently die.
Check for timeouts with external crystal, pll, or whatever is being used as the primary clock source.
2019-05-22 12:21 PM
What is connected to the NRST pin?
JW
2019-05-22 12:49 PM
If it is driven high (ie by a push-pull driver) then the part won't reset properly.
2019-05-22 1:38 PM
What IDE or programmer are you using to program the processor?
Some programmers are configured by default to just run to main() right after programming, and therefore, stop execution at main(), which appears to match your description.
2019-05-22 9:20 PM
Do you have some kind of boot loader? When you load the code with IDE, it starts from the beginning of the loaded image. Using reset makes it jump to the reset vector and so does starting the system without IDE. Well, at least that happens with Eclipse and its derivatives.
However, some time consuming HW start-up sounds more probable here.
2019-05-23 12:41 AM
NRST pin is connected to a capacitor to GND and also to a button that connects to GND when it is pushed. The problem is not in the NRST, because when I reset the MCU it works fine and executes the code. The problem is when I powerup the MCU that it doesn't start the execution.
A important remark is that when I'm debugging with Eclipse, the execution is donde properly. I don't understant what is happening.
Thanks you!
2019-05-23 12:44 AM
I'm using System Workbench for STM32 that is based on Eclipse. I don't know if it is configured to stop execution at main(). Where can I see this configuration?
However, it's important to notice that with other codes (and in the same IDE, programmer and board), the MCU works properly, code execution starts when it is power up). And also I want to remark, that when I debugging the code is executed also fine.
Thank you very much!
2019-05-23 12:50 AM
I'm using the startup file generated by the Cube software. (startup_stm32l476xx.s) amd the linker that also is generated by Cube (STM32L476RCTx_FLASH.ld). Certainly, I don't know where is the problem. It's important to remark that with other project codes the MCU starts code good (when it is power up and after reset). But with my current project, only starts execution after reset.
I have compared the startup and linker files, but they are the same. I don't know if it is a building configuration, of a configuration file, but I'm sure that is a firmware problem and not a hardware one, because with other projects it is working.
I don't know if it is important, but I have to say that I'm using FreeRTOS. But, I think that this is not involved in the problem.
Thank you very much!
2019-05-23 10:07 AM
It's a breakpoint setting command in the debug startup script.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.