2019-04-22 1:06 PM
Hello folks
This is my first time working on ST processor and USB and need some help I am using STM32F407VG Processor in the host only mode and standard peripheral library
I am not using SOF and using HSE as an input to the PLL operating at 168 MHz I enable the USB clock as well Is there anything special I need to do for LS mode
Hub used is USB2512aezg
Thank you in advance
2019-04-22 5:47 PM
There were rumors that STM32F4 does not support hubs, especially in low speed mode.
No official errata from ST, though.
-- pa
2019-04-23 7:20 AM
hmm Thank you Pavel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.