STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Code stucks at MX_USB_DEVICE_Init();

Hello, I use STM32F103C8Tx but USB communication does not work as it intends to. Sometimes codestuck at MX_USB_DEVICE_Init(); function.. More spesifically  it gets stuck atUSBx->BTABLE = BTABLE_ADDRESS; line inside of MX_USB_DEVICE_Init();When I con...

GunkutA by Senior
  • 833 Views
  • 0 replies
  • 0 kudos

Dual IPAddress support using LWIP

Hello All,I have a requirement where i want to use dual ip address on single MAC / Network interface. Is it possible using LWIP stack? IS this feature supported in LWIP? Any one aware of the challenges for the same.

AGupt.12 by Associate II
  • 1116 Views
  • 1 replies
  • 1 kudos

STM32G4 UCPD without RTOS?

I am interested in the UCPD peripheral built in to the STM32G431. However, I noticed that the software support for the peripheral requires FreeRTOS. Does anyone know of any support (or planned support) for the UCPD peripheral that does not require an...

jefflongo by Associate III
  • 1606 Views
  • 1 replies
  • 0 kudos

Fail to write to SD

Hi,I'm using STM32L451RCT with SDMMC and FATFS.I'm Generating the code from CUBE.Reading files (f_read) from SD is working but I'm failed to write to file (f_write)Does anyone know how can I solve the problem

Schar.1 by Associate
  • 1228 Views
  • 3 replies
  • 0 kudos

stm32l4xx_ll_rcc.h and stm32g4xx_ll_rcc.h wrong implementation of LL_RCC_PLL_ConfigDomain_SYS macro

Wrong original:__STATIC_INLINE void LL_RCC_PLL_ConfigDomain_SYS(uint32_t Source, uint32_t PLLM, uint32_t PLLN, uint32_t PLLR){ MODIFY_REG(RCC->PLLCFGR, RCC_PLLCFGR_PLLSRC | RCC_PLLCFGR_PLLM | RCC_PLLCFGR_PLLN | RCC_PLLCFGR_PLLR,       Source | PLLM |...

Robert1 by Associate II
  • 1197 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.