2023-03-27 8:04 AM
Cannot find LL_FLASH_ErasePage or LL_FLASH_WriteHalfWord ! Where I can find this ?
Adam
Solved! Go to Solution.
2023-03-28 7:39 AM
Then, I am sorry. I was a little bit ****** off. Lack of time.
Unfortunately I cannot share cause I get it under NDA.
Looks like I need to port it myself and I already hate it.
Actually not only port it, but also test it in all possible conditions.
2023-03-27 4:04 PM
Nowhere. Either use HAL, or better, instead of using a broken bloatware, write a normal code.
2023-03-28 6:12 AM
Are you from ST or just a man who loves to write own code for everything ?
Don't have time to work on ST homework.
I am moving aplication from STM32F0XX to STM32L0XX . I have LL driver for first , for second not .
Hey ST what's wrong with you ?
Same with STMCUBEMX. Some part's of code is generated. The other part is not. Just guest what is missing. ******* great idea.
You can say - use HAL. Sure why not - just deliver bigger devices with same price.
Concept is good. Driver library to not spent time digging registers. Just ,lost somwhere.
2023-03-28 6:30 AM
I find it very interesting that you can't find LL drivers for the STM32L0?
I find them for both the STM32F0 and the STM32L0 in their respective repositories.
However, I would be very interested to know where you found the LL_FLASH_ErasePage and LL_FLASH_WriteHalfWord functions for e.g. STM32F0 you mentioned?
If you use the libraries from STMicroelectronics, you don't necessarily have to do everything with HAL; you can also specify for almost all peripheral modules whether you use LL or HAL. In this respect, memory consumption can be finetuned quite well.
Of course, if you have a lot of time, you can save even more memory with bare metal programming - every user can put together his or her own personal way of working.
Regards
/Peter
2023-03-28 7:26 AM
Can you find stm32l0xx_ll_flash.h ?
I am looking for :
LL_FLASH_IsLocked()
LL_FLASH_Lock()
LL_FLASH_IsBusy()
LL_FLASH_StartProgramming()
LL_FLASH_StopProgramming()
LL_FLASH_StartPageErase()
LL_FLASH_StopPageErase()
LL_FLASH_SetAddress()
LL_FLASH_Start()
LL_FLASH_WaitForLastOperation()
LL_FLASH_ErasePage()
LL_FLASH_WriteHalfWord()
LL_FLASH_WriteWord()
Looks like LL library. Isn't from ST ?
I have stm32f0xx_ll_flash.h and it definitelly looks like one of yours.
From other hand I has no typical ST statment in comment at the beginnig.
2023-03-28 7:32 AM
No, even in my backups of very old libraries I can't find stm32f0xx_ll_flash.h. My favourite internet search engines also find exactly nothing for this file name.
Where did you get it from?
Can you please upload it so I can take a look?
2023-03-28 7:39 AM
Then, I am sorry. I was a little bit ****** off. Lack of time.
Unfortunately I cannot share cause I get it under NDA.
Looks like I need to port it myself and I already hate it.
Actually not only port it, but also test it in all possible conditions.
2023-03-28 7:48 AM
That's OK, everyone is under time pressure sometimes and scolds someone else. ;)
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.