2022-05-05 10:03 AM
I am working on a IoT product with the STM32L412CBU6 that requires flashing and testing at our manufacturer. I am able to program the device through DFU mode over USB using:
sudo dfu-util -a 0 -i 0 -s 0x08000000:mass-erase:force:leave -R -D firmware.bin
However, it does not enter back into regular mode. Even if I return the boot pin to low and reset, it still appears as a DFU device with lsusb. However, when I power cycle the device it behaves as if it has the new firmware, and I am able to update the firmware with the exact same script and set it to normal/DFU mode using the boot pin and reset.
My question is why does the dfu update work in EVERY other instance other than the very first time I flash the firmware?
2022-05-05 1:10 PM
Probably this http://www.efton.sk/STM32/gotcha/g44.html documented by @Community member :)
2022-05-06 3:09 AM
If this is problem, maybe the way out is through playing with the Option bytes.
Maybe inspiration:
JW
2022-05-06 11:22 AM
Why dfutil? STM32Programmer is better for this. And DFU protocol have command for run application , maybe this jump to app work.?
2022-05-06 12:37 PM
Thanks for the insight. I am going to look into programming the option bytes. It looks like dfu-util has this as an option.
2022-05-06 12:38 PM
I have to use the DFU protocol because that is the interface we selected in product development for updating firmware. I will investigate if the STM32Programmer can run on arm through the USB.
2022-05-07 1:10 AM
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0-RC1
-------------------------------------------------------------------
Usage :
STM32_Programmer_CLI.exe [command_1] [Arguments_1][[command_2] [Arguments_2]...]
Generic commands:
-?, -h, --help : Show this help
-c, --connect : Establish connection to the device
<port=<PortName> : Interface identifier. ex COM1, /dev/ttyS0, usb1,
JTAG, SWD...)
USB port optional parameters:
[sn=<serialNumber>] : Serial number of the usb dfu
[PID=<Product ID>] : Product ID. ex: 0xA38F, etc, default 0xDF11
[VID=<Vendor ID>] : Vendor ID. ex: 0x0389, etc, default x0483
UART port optional parameters:
[br=<baudrate>] : Baudrate. ex: 115200, 9600, etc, default 115200
[P=<parity>] : Parity bit, value in {NONE,ODD,EVEN}, default EVEN
[db=<data_bits>] : Data bit, value in {6, 7, 8} ..., default 8
[sb=<stop_bits>] : Stop bit, value in {1, 1.5, 2} ..., default 1
[fc=<flowControl>] : Flow control
Value in {OFF,Hardware,Software} ..., default OFF
Not supported for STM32MP
[noinit=noinit_bit]: Set No Init bits, value in {0,1} ..., default 0
[console] : Enter UART console mode
JTAG/SWD debug port optional parameters:
[freq=<frequency>] : Frequency in KHz. Default frequencies:
4000 SWD 9000 JTAG with STLINKv2
24000 SWD 21333 with STLINKv3
[index=<index>] : Index of the debug probe. default index 0
[sn=<serialNumber>]: Serial Number of the debug probe
[ap=<accessPort>] : Access Port index to connect to. default ap 0
[mode=<mode>] : Connection mode. Value in {UR/HOTPLUG/NORMAL/POWERDOWN
}
default mode: NORMAL
[reset=<mode>] : Reset modes: SWrst/HWrst/Crst. Default mode: SWrst
Reset mode with UR connection mode is HWrst
[shared] : Enable shared mode allowing connection of two or more
instances of STM32CubeProgrammer or other debugger
to the same ST-LINK probe.
[tcpport=<Port>] : Port used for running ST-Link Server, default 7184
SPI port optional parameters:
[br=<baudrate>] : Baudrate.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.