2021-04-12 5:14 AM
Hello, I downloaded STM32CubeExpansion_Audio_V1.1.1 and I tested the MP3 player project (Audio_MP3_player) with an STM32746G-Discovery.
It works very well.
But now, I would like to add 2 or 3 additional functions but I have big gaps in development.
I would like to add a speed or pitch function (+/- 10%) and a reverse play function.
When playing a WAV or MP3 file, the audio file is buffered before being played.
I think it's in the fwkmempool.c file or player.c file to add these functions but I can't seem to.
If anyone can help me it would be welcome.
Thanks for your help.
Regards.
2021-07-20 9:21 AM
Nobody ?
2021-07-20 10:30 AM
It's a forum, most people are occupied with their own projects and problems.
2021-07-26 8:22 AM
Update: I found out how to play an MP3/Wave sound while changing the playback speed.
Now I have to figure out how to play an MP3/Wave sound backwards.
2021-08-19 4:10 AM
Can you share your project here?
2021-08-19 7:14 AM
I'll send it to you later.
Thank you.
2021-08-19 9:43 AM
Here is the link to download my project written with keil for the STM32F7.
In the meantime I have managed to get the music speed to work at +/- 100%.
https://dedibout.fr/index.php/s/4ef22Rr43pATnpp
Thanks for your help.
2025-02-25 9:46 AM
Hi
Can you please reshare this project? It play music from USB Drive/SD card or transmited via USB from computer?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.