2016-10-27 3:20 AM
Hi everybody,
I am using a discovery eval board(stm32f4) with a 64-bit Win8.1 computer. I want to establish a serial commmunication via uart. So i have installed VCP software from STmicroelectronics website. But i see exclamation mark on the device in the device manager with error code:10. I am quite new with these discovery boards could you explain me what to do very simply?Thank you. #stm32 #usb #cdc #vcp #windows82016-10-27 6:10 AM
Hello,
I think this is related to the max_packet_size. Try to increase heap and stack sizes defined in startup_stm32f4xxxx.s fileRegards2016-10-28 2:07 AM
So, how can i access this file ? Where is it ?
2016-10-28 2:39 AM
Hi,
The startup files are here: STM32Cube_FW_Fx_Vx.x.x\Drivers\CMSIS\Device\ST\STM32FXxx\Source\Template(depending on used IDE).In your case for STM32F4: STM32Cube_FW_F4_V1.13.0\Drivers\CMSIS\Device\ST\STM32F4xx\Source\Templates RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.