2010-04-08 11:04 AM
UML / State diagram code generation tool
#rtos #code-generation #qp #stm32 #state-machine #state-machine #uml2011-05-17 4:46 AM
I've not used their code-generation capabilities, but have found both VisualState from IAR and Enterprise Architect from Sparx systems to be pretty good for the modelling:
http://www.iar.se/website1/1.0.1.0/1389/1/
http://www.sparxsystems.com.au/products/ea/index.html
VisualState, as the name suggests, is just about sate machines, and is specifically targetted to embedded systems. It is expensive. Enterprise Architect is (more of) a full UML tool, and not specifically embedded. It is inexpensive.2011-05-17 4:46 AM
Hi Kasper
I have been using Quantum Leaps' state machine framework on the STM32 with great success - see
. I heard through he grapevine that they are working on a code generation tool for their framework - not sure when it will be available.You can also have a look at www.umlet.com - they have a free drawing tool that works great for designing state machines, etc. No code generation unfortunately.
Hope this helps.
Gawie
2011-05-17 4:46 AM
Update: Quantum Leaps offers now a
free, cross-platform, graphical UML modeling tool called QM? (www.state-machine.com/qm) for designing and implementing real-time embedded applications based on the QP state machine frameworks. QM? provides best-in-class, intuitive diagramming environment and generates very compact C or C++ code that is 100% traceable from your design. QM? is currently available for Windows and Linux (Mac OS X is planned in the future).
The code generated by QM works on the STM32 microcontrollers. For more information about STM32, visit www.state-machine.com/arm.
2016-10-28 12:37 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.