2025-12-19 2:12 PM
Hi, I'm currently working on a project with an H755 board.
The project uses UART communication. I'm developing it on a Windows 11 computer, and it generally works fine on that computer. So far, there are no issues.
However, after completing the project, I'd like to be able to use it on my older laptop (currently running Windows 10 with ESU). Here's the problem: my Windows 10 computer doesn't recognize the STLink virtual COM port. It only sees the device as a standard COM port with a Microsoft driver (not ST Microelectronics), and its UART communication then doesn't work.
I don't have CubeIDE installed on my laptop. I don't need it on this computer. Should I install the driver manually? If so, where can I find it? Any ideas on how to solve this problem?
Solved! Go to Solution.
2025-12-19 3:09 PM
Worth a shot:
STSW-LINK009 | Software - STMicroelectronics
2025-12-19 3:09 PM
Worth a shot:
STSW-LINK009 | Software - STMicroelectronics
2025-12-19 3:43 PM
Thankst, this is exactly what I needed. Now works fine on older machine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.