2011-07-21 4:57 AM
Hello,
we are using an STM32F105 as USB device in conjunction with a special configuration program, that runs on a PC. If we use a PC with Windows XP, the USB driver is automatically installed and all works fine. But if we try the same with a PC running Windows Vista or 7, a driver is NOT automatically installed and the device is marked as 'not working'. The only way to avoid this, is a prior installation of the 'dfuSe' package. After installation of this package, the USB connection works, if you connect the MCU and the PC. Is there any other way (for driver installation), without prior installation ofthe 'dfuSe' package ? Thanks for all answers ! Regards moardy #usb-virtual-com-port #stm32-usb #windows-7 #windows-7 #windows-vista #usb #vcp #usb
2011-07-29 12:35 AM
THX, you make my day !
2011-11-02 7:32 AM
How can I make it work with Windows 7 Embedded Standard ?
This is important for me, my application needs WES7. Please help me. Thank you, Kind Regards, Tomasz Polus2012-05-30 6:55 PM
Hi, The following link doesn't work
http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/vcpdriver_v1.zip
I found it diffcult to find a useful thing on the internet , I'm very disappointed to ST, they don't really care the customer, what they care is sales, money!2012-05-31 4:38 PM
http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/stm32_vcp.zip
Cheers, STOne-32.2012-12-25 11:12 PM
Hi, are there any STM32F1 Windows drivers for other USB classes than virtual com port? If yes, can you provide the link to download? Thank you~
2013-05-30 4:42 AM
This link is out of date. So, where can I find the VCP drivers?
2013-05-30 5:10 AM
http://www.st.com/web/en/catalog/tools/PF257938
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.