2013-05-29 9:43 AM
The OpenBLT bootloader now supports making firmware updates from a Motorola S-record file stored on an SD-card. It uses Chan's FATFS module for file access.
Firmware updates are now as easy as: (1) store S-Record on SD-card, (2) insert SD-card in slot on microcontroller board, and (3) press reset. Everything else is done automatically.The OpenBLT download package contains demos that support firmware updates from SD-card for the following boards:We’re moving the ST Community to a new platform to give you a better and more reliable community experience.