STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB HS in FS + Internal DMA

Posted on May 03, 2013 at 07:46 Hi All, I have just started developing on the STM32 F4 Discovery with the purpose oftransferringdata from one incoming DMA (ie camera source) and out USB to a host PC. I have managed to get the USB examp...

tree by Associate
  • 1647 Views
  • 3 replies
  • 0 kudos

USB VirtualComPort Loopback

Posted on May 14, 2013 at 14:04Dear collegues, I experience a trouble with writing code for STM32L152VBT. Let me explain sequentially. I had my PCB with chip STM32L152VBT. I took the example project from STM32_USB-FS-Device_Lib_V4.0.0 and adopt to m...

Ivan by Associate II
  • 1419 Views
  • 3 replies
  • 0 kudos

Audio via USART (STM32F4 Discovery)

Posted on May 07, 2013 at 03:07I'm trying to create a project where I send an audio file from a computer to my STM32F4-Discovery board via USART and play the file. I have successfully run a USART example where a character is sent to the F4 board and...

Ethernet protocol

Posted on May 03, 2013 at 01:48Hello everybody, I have a stm3210E eval board and I want to design a project which contains an ethernet port.I know that this board doesn't support ethernet port.could I add any external ICs to this board to have ether...

STM3210C-EVAL - USB examples

Posted on April 24, 2013 at 10:30Hi, I'm getting started, would like to see some USB / PC interfacing. I have the STM3210C-EVAL, I'm using IAR and JLINK and have my own project compiling and running ok.I downloaded the doc at http://www.st.com/st-we...

ian239955 by Associate II
  • 4114 Views
  • 14 replies
  • 0 kudos

any commercial boot loader for STM32F103?

Posted on April 29, 2013 at 17:16We need a boot loader for customers to update the firmware. The product can't provide the BOOT0 pin, so the ST build-in boot loader can't be used. I am wondering if any commercial boot loader by using UART is availab...

huiyan by Associate
  • 1515 Views
  • 2 replies
  • 0 kudos

USB disconnect performence

Posted on April 28, 2013 at 14:12I have a problem when I use the USB in the Boot application and then jump to my main app without detach the USB . On the main I open it again but the other side lost connection in between. I try to stop the clock to ...

Barbie by Associate II
  • 1029 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.