2021-09-24 10:37 PM
Hi!
With the use of USB FS I want to design application & emwin on board stm32h743i-eval. When usb is attached, the function of enumeration does not work. Function USBH_Get_DevDesc get back as USBH_BUSY always and USB is found in condition of ENUM_IDLE. In case if I give remarks that function GUI_Init enumeration works good and some of the usb descriptors can be seen on uart terminal. Something stopping usb that is taking place in GUI_Ini .It’s strange that USB (HS) Host camera device working well with or without GUI_Init.
Following code functions well:
SystemClock_Config();
__HAL_RCC_CRC_CLK_ENABLE();
//GUI_Init();
USBH_Init(&usb_storage_handle, usb_storage_process , USB_STORAGE_ID);
USBH_RegisterClass(&usb_storage_handle, USBH_MSC_CLASS);
USBH_Start(&usb_storage_handle);
while (1) {
USBH_Process(&usb_storage_handle);
}
But USB stops working If I make changes in
//GUI_Init();
on
GUI_Init();
Kindly help me in this issue.
Thanks
2021-10-06 8:54 AM
Hello @LElla.1 ,
From what I understood you have an application that uses stmwin with USB and you faced problem of enumeration.
Can you please share more details about your issue?
Thanks in advance.
BeST Regards,
Walid
2021-10-12 8:27 AM
Hello @LElla.1
Are there any news concerning this issue from your side?
BeST Regards,
Walid
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.