2021-09-28 6:39 PM
Thank you for helping.
The microcomputer is STM32F769I.
I wrote the code with reference to the HttpServer sample.
TCP / IP server application.
When I send a packet from a TCP client, I can receive it, but then it HardFaults.
It seems to happen after releasing a semaphore with an Ether interrupt.
What could be the cause and how should I debug it?
Thank you.
2021-09-30 6:00 PM
Looking at the Hard Fault Handler is going to tell you nothing.
You'd do better with a routine that unpacks the failure state,and then look at the code that was faulting and the registers at that time.
Look at a disassembly view of the failing code, match it to the C code you compiled, and work back up the call-stack from there.
What structures, what pointers, and if memory has been released, etc.
2021-10-12 5:11 PM
Hi Tesla DeLorean
It was working at the time of FreeRTOS Ver1.
I'm using Ver2 now.
But I don't know if it's a Ver2 problem.
Now I don't have time to track in other jobs.
Thank you for your response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.