2025-04-15 5:01 AM - last edited on 2025-04-15 5:57 AM by Andrew Neil
Hi, I am curious one thing when using the HAL libraries. Just as an basic exapmle i assign LED1 to PB12 pin of STM32F070CBT6 as an GPIO_output. And i want to use HAL_GPIO_WritePin(GPIOB, LED1, LED1_SET); instead of HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET); . Do you think it is weird that i want to use my variables like that with HAL libraries? Second thing is (if it is not weir or inappropriate), should i define my definitions as "definitions.c" or "definitions.h"? When i make some search, .c file is not recommended. I am not sure if i do all these steps with my ST microcontroller and it works well.
Solved! Go to Solution.
2025-04-15 6:01 AM
@TDK wrote:Your usage mixes this with LED1_SET. But up to you.
It can be a good thing to define your own LED_SET and LED_CLEAR (or whatever) - this allows you to be independent of whether the LED is active-high or active-low.
Probably better names would be LED_ON and LED_OFF - which directly indicate the intended function, rather than hiding between the rather ambiguous "set" and "reset"...
2025-04-15 5:50 AM
> Do you think it is weird that i want to use my variables like that with HAL libraries?
A bit. The intended usage is something like:
HAL_GPIO_WritePin(LED1_PORT, LED1_PIN, GPIO_PIN_SET);Your usage mixes this with LED1_SET. But up to you.
> should i define my definitions as "definitions.c" or "definitions.h"?
They will need to be in a header file if you want to use them in multiple source files. If you're only using them within a single source file, you can put them in that source file. Up to you.
2025-04-15 5:57 AM - edited 2025-04-15 6:03 AM
@tensaisakuragi06 wrote:i want to use HAL_GPIO_WritePin(GPIOB, LED1, LED1_SET); instead of HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET); . Do you think it is weird that i want to use my variables like that with HAL libraries? .
Of course not!
That is exactly what CubeMX does with its generated code, and what many ST BSPs (Board Support Packages) do, too.
HAL_GPIO_WritePin is just a C function - its parameters work exactly the same as any other C function.
BTW: note that it is usual practice for ALL CAPITALS names in C to be reserved for #defined names - not variables.
@tensaisakuragi06 wrote:should i define my definitions as "definitions.c" or "definitions.h"? .
You can name your source files however you like!
But you need to understand the C rules of scope & visibility - this is standard C, and nothing specifically to do with STM32.
When you say "definitions", are you talking about preprocessor definitions (using #define), or C functions & variables?
With functions & variables, be sure to understand the difference between declarations and definitions:
@tensaisakuragi06 wrote:When i make some search, .c file is not recommended.
Please provide examples - you may be misunderstanding.
@tensaisakuragi06 wrote:I am not sure if i do all these steps with my ST microcontroller and it works well.
This is all standard C stuff - nothing specifically to do with ST or even microcontrollers.
Here are some C learning & reference materials:
https://blog.antronics.co.uk/2011/08/08/so-youre-thinking-of-starting-with-c/
2025-04-15 6:01 AM
@TDK wrote:Your usage mixes this with LED1_SET. But up to you.
It can be a good thing to define your own LED_SET and LED_CLEAR (or whatever) - this allows you to be independent of whether the LED is active-high or active-low.
Probably better names would be LED_ON and LED_OFF - which directly indicate the intended function, rather than hiding between the rather ambiguous "set" and "reset"...
2025-04-15 7:26 AM
I define them with header file format (.h). It works for now. Thank yu for your pointers.
2025-04-15 7:30 AM
Yeah, it stil confuses me sometimes, i am planing to use both #define 's and variable definitions like unsigned int16 ... ;
According to your pointers, i should seperate them like "declarations for #define 's " and "definitions for unsigned int16 ... ; " like. I hope that i understand you correctly :) .
2025-04-15 7:30 AM
@tensaisakuragi06 wrote:I define them with header file format (.h).
That doesn't really make sense - a header (.h) file has no "format" different from a .c file.
The difference is in the way they are used - not their "format".
2025-04-15 7:33 AM
// Pin definitions
#define LED1 GPIO_PIN_12
#define LED2 GPIO_PIN_3
#define ROLE1 GPIO_PIN_7
#define ROLE2 GPIO_PIN_6
#define BUTON1 GPIO_PIN_13
#define BUTON2 GPIO_PIN_14
#define BUTON3 GPIO_PIN_15
// Macro definitions
#define LED1_ON GPIO_PIN_SET
#define LED1_OFF GPIO_PIN_RESET
#define ROLE1_ON GPIO_PIN_SET
#define ROLE1_OFF GPIO_PIN_RESET
#define LED2_ON GPIO_PIN_SET
#define LED2_OFF GPIO_PIN_RESET
#define ROLE2_ON GPIO_PIN_SET
#define ROLE2_OFF GPIO_PIN_RESET
#define BUTON1_ON GPIO_PIN_SET
#define BUTON1_OFF GPIO_PIN_RESET
#define BUTON2_ON GPIO_PIN_SET
#define BUTON2_OFF GPIO_PIN_RESET
#define BUTON3_ON GPIO_PIN_SET
#define BUTON3_OFF GPIO_PIN_RESET
2025-04-15 7:34 AM
I change my definitions like above and its looks good for me. If i can improve my logic, please do not hesitate to tell me.
2025-04-15 7:40 AM
@tensaisakuragi06 wrote:According to your pointers, i should seperate them like "declarations for #define 's " and "definitions for unsigned int16 ... ; " like. I hope that i understand you correctly :) .
I'm afraid not.
#define is used by the preprocessor; it is purely text substitution. It never gets seen by the compiler proper.
Definitions for functions & variables are what actually create the objects (data or code) in memory. The C programming language requires that each functions & variable must have exactly one definition.
Having more than one definition of a function or variable is an error - you will get an error message saying, "multiple definitions".
Declarations for functions & variables do not cause any memory to be allocated, or code created - they simply give enough information for the function/variable to be used, on the assumption that it has been defined somewhere else.
Again, this is all standard C stuff - nothing specific to ST or embedded or microcontrollers - so see general C programming tutorials, textbooks, etc for details.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.