2024-08-20 4:41 AM - edited 2024-08-20 4:51 AM
Hello,
I'm working on a project which includes: W25Q32 (NOR Flash), File system and USB MSC + CDC on STM32U0 series MCU - STM32U073RCT6.
Till now, I've implemented these:
- SPI setup and communication with the NOR Flash (W25Q32)
- For the file-system part, I tried to do it using the FileX but couldn't find relevant resources for "FileX + NOR Flash + SPI + STM32U0 series MCU". So, I found this https://github.com/maxiufeng258/SPI_Flash_Uart_Led_Polling_V1.0 (FatFS + W25Qxx) and implemented the same for my MCU as well. And able to create and mount the file system, create folder, text file and able to scan the disk.
- Next for the USB part, I've seen some articles and videos, implemented CDC-ACM using USBX and my laptop (USB host) is able to load the appropriate driver for my MCU (USB device) and able to perform CDC-ACM i.e tested by sending some random text from MCU to laptop.
- Now, I want to implement the MSC part as well. But the thing is, I think it'll become difficult to integrate all these: FatFS on W25Q32, USBX CDC and this MSC part.
- So, can any provide me any suggestions on how to move forward and provide some references if any?
Once again specifying me requirements:
- Basically, I'm working on a Temperature Datalogger. For every certain interval, the temperature sensor will collect data and store it in internal SRAM.
- And after storing some points on SRAM, I move the data to internal Flash.
- And then, in the end (after certain data points) I want to move all the data from internal flash to external flash memory.
- I'm using w25q32 which is a NOR Flash memory. I've implemented SPI communication with this.
- And then instead of using FileX + LevelX, I used an external FatFS library and done the file system part and created a folder (and a text file in it)
- Now, these things are left:
1) Moving data from internal flash to W25Q32 NOR Flash
2) Formatting this data into a CSV file and keeping it inside a folder in w25q32 using the FatFS library I used above
3) And then the USB part i.e When I plug-in the device via USB into the laptop, I should be able to see the CSV file.
2025-08-04 4:56 AM - edited 2025-08-04 4:57 AM
Hello @RB4020
Have u completed this one? because i am also facing same problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.