2026-01-12 6:49 AM
I am using a UX_Device_Audio2.0-based project on H7.
Could this be a codec configuration issue (mixer/settings), a USB audio packet scheduling problem, or something else? I can't seem to find a fix yet.
Solved! Go to Solution.
2026-01-20 8:03 AM
Hello @FBL
The issue was the cable. It was mixing two channels together thus not giving a true stereo output.
Once I changed the cable, it worked as normal.
Thanks.
2026-01-12 6:53 AM
> Could this be a codec configuration issue (mixer/settings), a USB audio packet scheduling problem, or something else?
Yes, yes, and yes.
Hard to guess without any info - except that it doesn't work.
2026-01-12 7:06 AM
LOL - that's funny, thanks for the laugh.
This can be tested with base example from STM32 - I just tested it on H753i-eval board.
2026-01-12 7:58 AM
... which surely everybody has and uses it that way?
;)
At least we have one more info now.
2026-01-12 9:08 AM - edited 2026-01-12 12:00 PM
>This can be tested
- I dont have this board.
- what sample rate you set ? Try 48k 16b stereo. (USB /UAC1 only working correct at 48k...afaik. Maybe UAC2 can do more...but i never tried, lost interest /too much to learn and check and program then )
- what you set/tried at host side ? + host is...Win/mixer , Linux/Alsa , pulse.., pipe ..or ?
2026-01-14 2:07 AM - edited 2026-01-14 2:09 AM
Hi @audio
Thank you for providing your feedback regarding this issue.
Did you play test signals from PC :a left-only /right-only sine, a dual-mono tone ?..
To better isolate the root cause, do you reproduce using this example Projects\STM32H743I-EVAL\Examples\SAI\SAI_AudioPlayback and can you log a few frames of what you receive into a small array and inspect via debugger or UART .
Your symptoms are more likely coming from codec mixer /analog routing or digital channel mapping (USB buffer to SAI) rather than USB packet scheduling.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-20 8:03 AM
Hello @FBL
The issue was the cable. It was mixing two channels together thus not giving a true stereo output.
Once I changed the cable, it worked as normal.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.