STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L0 Uart failure after OTA

hi,Previously i was using STM32L010K8TX which has 8K memory. I did OTA update in this device via Uart with help of external controller which receive hex file from User. Currently am using STM32L010R8Tx which has 64K memory. And i tried the same OTA p...

nikhivv07 by Associate II
  • 5426 Views
  • 10 replies
  • 2 kudos

STM32L4 XMODEM using USB CDC Interface

Posted on February 03, 2017 at 17:57I'm trying to implement an XMODEM file transfer through the USB CDC Interface on an STM32L4 processor in Full-Speed and seem to be having issues with XMODEM 132 byte packets getting split up and one of the middle ...

jacob2 by Associate III
  • 1380 Views
  • 1 replies
  • 0 kudos

TCP Socket bare-metal, can it be done?

Hi,I am running a simple TCP server using the lwIP stack and no RTOS. I got help from the "Echo_Server" example offered in most ST eval board packages, everything works fine.I need to accept a single socket connection from the outside and maybe also ...

AndrewST by Associate II
  • 5823 Views
  • 13 replies
  • 1 kudos

Interfacing Multiple ADC Channels for Data logging

Moved from TouchGFX forumGreetings Community,                                   I need advice on data logging multiple ADCs and/or ADC Channels to interface 40+ Train Gauge Values on an MCU that can show data on LCD or transmit Data over USB or seria...

Caan by Senior
  • 2397 Views
  • 7 replies
  • 0 kudos

Resolved! CMSIS RTOS v1 Semaphore Problems

Hi, I have a problem with CMSIS RTOS v1 using STM32F103RET6. I have about 6 - 7 tasks. The first task is the StartDefaultTask, after finishing initializing, when running to osSemaphoreRelease, it gets to configAssert(pxQueue) and loop forever. The se...

bl1ndf0ld by Associate II
  • 2181 Views
  • 4 replies
  • 0 kudos

USB OTG Dual Role

Hi STM Team, I am using STM32H723ZGT6 Microcontroller for my new project, I am using Azure RTOS for My application.I required to copy my data to Pendrive (I am using USB Host Only Mode and USBX and FileX).As well as i also required to use USB CDC ACM...

rkuma.21 by Associate III
  • 1168 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L433 CAN filtering using mask mode

Hello, I am currently using a STM32l433 with the following configuration: CAN_FilterTypeDef CAN_FilterInitStructure = {0}; CAN_FilterInitStructure.FilterBank = filterNum; CAN_FilterInitStructure.FilterScale = CAN_FILTERSCALE_...

agennart_0-1744871209560.png
agennart by Associate II
  • 4141 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.